I am in the midst of prototyping a couple of boards using the ADS7951.
Starting on page 34 of the data sheet, the example circuits mark the REF5025 part as "o/p" which implies that it is an optional part. The text states that the chip "can operate with an external 2.5V ± 10mV reference."
I just want to clarify what the options are. While the data sheet says it "can" operate with a part like the REF5025, it's not precisely clear about whether the chip can operate without it. Besides 2.49V to 2.51V external, is there any kind of internal reference at all? Can the pin be tied to 5V instead, like the analog supply? Are there really any usable options for a 12-bit AD?
Better text might be to say that the reference is not optional, but rather it must be used, or something equivalent or similar.
One part I have been using is the Vishay Si9183DT-25, which provides 150 mA of reference current at 2.5V for one-tenth the cost of the REF5025, so I am wondering if anyone has used this ... or would it compromise the accuracy of the 12-bit converter?