I am looking for a replacement for the ADS7824P.
I need the same input and conversion capability (number of bits) but I need a smaller package (serial only).
Only one A/D input OK, prefer four.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joseph,
The ADS7824 is also available in the SOIC. There are also other possible options for a 4-Ch 12 bit SAR ADC:
ADS7841, 4 Single -Ended channels/2 differential channels, Serial SPI interface, SSOP-16, 200kSPS
ADS7924, 4 SE channels, I2C interface, 3x3QFN 16, 100kSPS
TLV2544, 4 SE Channels, Serial SPI interface, SOIC-16, TSSOP-16, external or internal reference, 200kSPS
TLC2554, 4 SE Channels, Serial SPI interface, SOIC-16, TSSOP-16, external or internal reference, 400kSPS
Thank you and Best Regards,
Luis
Hello Joseph,
My apologies, I missed the +/-10V input requirement.
The ADS8512 single channel 12 bit +/-10V range with serial interface on SO-16 package, supporting 40kHz sampling rate. The ADS8508 is a 12Bit +/-10V single channel with serial interface device available on the 20 pin SO package, supporting 250kSPS . The ADS8519 is a 16 bit device available on the 28 pin SSOP package.
Best Regards,
Luis