Hi,
Currently I design a data logger board which need 4 channel analog input. I use 4 ADS1222 and one MSP430F5436A. Now I have some questions need clarify. Please help, thanks in advance.
1. To accomplish analog input range +-5V, the Vref is 2.5V and VDD is 5V. According to ADS1222 spec page 4, VOH will be 0.8VDD min, that is 4.0V min in my design. Can the MSP430F5436 accept 4.0V digital input? I see reference schematic in ADS1224 is direct connect to MSP430. If not I will add a buffer between ADC and MSP430.
2. Since there are 4 ADS1222 on board, do I need use 4 voltage reference (ref5025) to 4 ADS1222 or one ref5025 to 4 ADS1222?
Elite Hsieh