This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash Memory usage as Data Memory with write enable feature

Other Parts Discussed in Thread: MSC1210Y5

Hi,

I am using TI - MSC1210Y5 data convertor. It has 32KB of Flash with 1024 bytes of SRAM.

The scenario is, I would like to use 32 KB of Flash as 16KB program memory and 16KB data memory. I would like to know, will this 16KB data memory be read-only ? OR I could use 16KB data memory for as much as possible read and write operation during code/application execution inside the hardware.

For example: If I define an integar variable  (say ExampleIntegar) in the 16 KB data memory (in FLASH), could I be able to assign new values (multiple time) to this variable during the code/application execution?

If the data memory could be re-written multiple time during program execution, then which register settings should I use to configure 16KB daa memory and 16 KB flash memory ?

 

Please guide

 

Regards

Asad