HI my customer would like to use two ADS7945 in parallel.
He would like to read both measurments at the same time and would like to know the jitter between both measurments.
could you please help?
regards
kamal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI my customer would like to use two ADS7945 in parallel.
He would like to read both measurments at the same time and would like to know the jitter between both measurments.
could you please help?
regards
kamal
HI,
Any body can answer the following question?
Regards
Kamal
Hi Kamal,
I apologize for the delay. Aperture jitter is not something that is characterized on this part. The datasheet only specifies a typical value of 10ps (RMS) based on simulation. If two ADCs are being used for simultaneous sampling then the RMS jitter between their measurements would just be ((10ps)^2 + (10ps)^2)^(1/2) ~= 14ps or +/-42ps worst case assuming a factor of 3 for a Gaussian distribution. Of course this is assuming the clock signals driving the sampling switches of the two ADCs are in-phase and precise (jitter << 10ps) so that their contribution is negligible.
Best Regards,
Harsha Munikoti