This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400 + AFE5805

Other Parts Discussed in Thread: AFE5805

I need some information about TSW1400 to see if I should buy it to my project.

I have AFE5805 and a TSW1250 but I need get the 8ch simultaneously, I will need a diferent adapter or TSW1250-AFE58XX works for it?

I will need to develop a code to fire the transducer making a beamforming. Actualy I already did that on a FPGA altera, but i will need to put all the things (emition and reception) on the same TSW1400 FPGA. The board can do it?

To make the High Voltage Emission I have a HV758 Supertex board. Do TI have a board to make the emission like that one? 8ch and dont need to be arbitrary shape.

Thank you

Danilo Câmara

  • Danilo,

    1. The TSW1400 can capture 8 channels simultaneously, while the the TSW1250 cannot.  The adapter for the    AFE5805-TSW1250 will also work with the TSW1400. 

    2. Yes,  you would have to write FPGA code for this, but you can use the CMOS connector on the board to generate stimulus signals for the transmitter. Simultaneously, you can capture data on the LVDS connector.

    3. Please look at this option:  http://www.ti.com/tool/tx-sdk-v2

    Thanks,

    Chuck Smyth