Other Parts Discussed in Thread: DAC5687, TPS51020, TPS40007
Although the customer is evaluating DAC5687, the following operations have occurred.
If a cause is known, please let me know.
------------------------------
[Phenomenon]
- Where the SLEEP pin of DAC5687 is set to High(Active), set up the register of DAC5687 by a serial signal.
When a setup is completed, a SLEEP pin is canceled (Low) and data is inputted into DAC, it may not be obtained with the time of an output being obtained from DAC.
After activating a SLEEP pin in that case, an output may be obtained if it cancels.
If this operation is repeated several times, the time of not being obtained with the time of an output being obtained will come out.
[Setup]
- As for a serial clock, 5 MHz
- TXENABLE and QFLAG are High
- PLL VDD is GND connection.
- PLL LOCK is intact.
(It was outputted to High)
[My idea]
Input power sources are the following devices.
- DVDD(1.8V):TPS51020
- AVDD(3.3V):TPS40007
Having inputted into AVDD with the DC-DC converter, I think that the inside DAC is affected.
------------------------------
Thank you for your consideration.