This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7954 / about pin connections

Guru 20090 points

Other Parts Discussed in Thread: ADS7954

Hello,
 
Could you please let me know reccomended  pin connections of ADS7954 TSSOP PKG ?
 
(1) GPIO1~3
Should we pulled up or pulled down these pins?
If yes, please let me know recomended resistor value.
 
(2) SDO, SDI , SCLK, CS
I believe that these pins don't need pullup or pulldown.
Is my understanding correct ?
 
(3)NC pins
Should we connect to GND ?
 
Best Regards,
Ryuji Asaka
  • Ryuji-san,

    Please see the responses for each set of pins below:

    (1) GPIO1~3

     By default, these pins are configured as inputs. If their state is not explicitly changed, a weak 1M pull down could be used on these inputs to park them to a known state. However, if the function or direction is changed (GPIO 3 supports an active low PD on the TSSOP package, for instance) care needs to be taken to ensure that the external pull resistor does not conflict with the device functionality.

     (2) SDO, SDI , SCLK, CS

     You are right. No pull-up or pull-down is required.

     (3)NC pins

     NC pins may be shorted to GND.

     Regards,

    Sandeep