Assuming a setting of both single ended and differential inputs, with 0-5V input range, having an external reference, VA=5V, and VIO=3.3V, could we get clarifications on the following:
- If the buffer is OFF, would we still be able to measure thermistors, RTDs, and other high impedance sensors?
- Is unipolar measurement only for gains of 8 or below (buffer=Off.) With a gain of 16, there seems to be some overlap in possibilities for the VINN max and VINP min
- Would the resolution for a unipolar input of 0-5V just be 23 bits?
- What is the wake-up time out of stand-by?
- For system calibration, is a full-scale input required throughout? It seems to mention that it might not be required, and with this in mind, could a gain coefficient be calculated with a 4V reference input, when the plan is ultimately to use 4.99V for the reference?
Any answers that can be provided would be greatly appreciated!
-Reagan