Hello,
I need to sample an amplitude modulated signal with a carrier frequency of 100kHz and band with of 200Hz with a resolution of 24bits. I need 3 channes with this characteristics, and would like to have it in one chip.
I wonder if :
A : is there any of your microprocesors or DSPs with at least 3 ADC 24bit and sampling frequency > 200kHz ?
B : AN other option is a so call Bandpass sigma-delta converter (from analog documentation MT-023 page 9 [1]) is there any system that includes this and/or allows to implement this?
C: is there any other possible solution that I'm missing ??
Thanks.