Hello,
I am having an issue using the external trigger on the TSW1400EVM. The external trigger only works about 75% of the time and I have spent hours trying to debug whether this is an issue with the High Speed Data Capture software or the board itself with no results. I have verified that the external trigger pulse is being delivered to the board and have tried many different signal levels from 2.4V-5V. In each case the pulse is correctly delivered to the board and sometimes it will trigger and other times it won't (seems to be random, but I would have a tough time accepting this).
Has anyone else seen something like this?
Thank you,
Thayne