Hello Team,
I would like to ask the following questions.
(1)
Could you tell me the Rint setting values when IAUX_DAC=5mA、Rext=300Ω and Full Scale=1.5V?
Because Rext and FS AUX DAC setting values is written but Rint isn't written in the following sentences(P.90 of AFE7222 datasheet).
"For best linearity, limit the maximum voltage at AUXDAC_A to 1.5V.For example, with I AUX_DAC set to 5 mA, and R EXT set to 300 Ohm, the voltage on AUXDAC_A will swing from 0 to 1.5V."
(2)
I believe Rint is connected in parallel with Rext.
Could you tell me whether Rint affects the formula(AUXDAC_A=IAUX_DAC x REXT)?
"For maximum input code, voltage on AUXDAC_A is equal to IAUX_DAC x REXT."(P.90 of AFE7222 datasheet)
Best Regards,
Hidetoshi Matsunami