Hi All.
I am in the process of using the ADS930 ADC, and I would like to be able to tristate the digital outputs, or put them in a high impedance state, in order to also be able to write to an LCD screen that will be connected to the same digital I/O lines.
I plan initially to sample for some milliseconds, and then process the results, before starting to collect more samples. Whilst not collecting data I plan on putting the digital outputs in the high impedance state, and at this point update the LCD.
My question relates to how the data sheet is worded, which is as follows.
“The digital outputs of
the ADS930 can be set to a high impedance state by driving
the OE (pin 16) with a logic “HI”. Normal operation is
achieved with pin 16 “LO” or Floating due to internal pulldown
resistors. This function is provided for testability
purposes but is not recommended to be used dynamically.”
Does this mean that the high impedance state feature is not recommended in operation, and in fact this ADC cannot put its digital outputs in high impedance state?
Kind Regards
Martin