This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7222

Hi all,

1. I would like to know, is there anyway to connect AFE7222evm with  PC without any FPGA device,(using uPP )

2. Is there any way to connect MatLab Simulink direct to AFE7222EVM?

Thanks ,

Sargis Sargsyan

  • Hi Sargis,

    1) The uPP interface requires single ended CMOS signals whiles the AFE7222EVM was built to use differential signals from the LVDS connector. Connecting the two interfaces is therefore not possible.

    2)  There are drivers available in <HSDCPRO install directory>/HSDCPro Automation dll folder that can allow you to connect to Matlab but the AFE7222EVM needs to be connected to the TSW1400EVM.

    Thanks,

    Eben.