Hi,
I am working on a design with and ADS8864. The analog section has some signal condition with a couple of amplifiers and a voltage reference with no shutdown pins. The problem is, I need to shut down the analog section for extensive periods of time while keeping the digital section powered. The options I can think of are:
a) Shut down the analog section including AVDD using a load switch but keep DVDD powered up. There is no information on power sequencing in the data sheet so I am not sure if this isn't going to damage the device. Also I am not sure if there will be increased leakage currents.
b) Shut down the analog section including AVDD and DVDD of the ADS8864 using a load switch. In this case the SPI lines would remain connected to the uP which will remain powered all the time.
c) Replace the OPAmps and voltage reference with similar ones but with shutdown.
Which one is the best solution and most importantly, which has the loses average current consumption?
Many thanks in advance for your help.
Christof