This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the output timing of DAC3152.

Guru 19245 points
Other Parts Discussed in Thread: DAC3152

Please let me know below about the output timing of DAC3152.

 

--------------------------

The following is written on the 7&14th page of the datasheet.

・Ach is a rising edge of DACCLKP.

・Bch is a falling edge of DACCLKP.

・Latency is typ 1.5 cycle. (Input=>Output)

 

In this case, the timing of output:(1) or (2),which is right?

(1):The output is update simultaneously about IOUTA/B.

(2):The output side is update individually about IOUTA/B.

※The image figure should look at attachment.

--------------------------

 

Best regards,

Satoshi