Dear all,
We are using ADS1230 and DAC161P997 in one of our application which consist of PIC16f1938 controller.
Our application as follows,
* ADS1230 is used to read the data from the loadcell for calculating the weight by the controller.
* DAC161P997 is used to convert the weight data to analog output (4 -20 mA). Weight data sent by the controller to DAC as the given format.
We are facing the problem as follows,
* When we are reading the ADC value from the ADS1230 then DAC output is dropping. ie if the Actual value of the DAC Output is 20mA. But during this time it is giving only 18.9 mA. If we didn't read the ADC data then DAC is giving the 20mA.
For example, If we sent the value 54610 to the DAC, then the output of the DAC is 20 mA (when we stops receiving the data from the ADC, stop sending the SCLK to ADC). If both the tasks runs simultaneously mean reading the data from ADC and sending the data to DAC then the DAC output is dropped to 18.9 mA.
But, above all conditions the weight value remains the same ( no dropping or no increase of weight). we didn't understand that why it is dropping the DAC output.
Please give us the solutions for the same.
Regards
K.Vinayagamoorthy
LCS Controls Private Limited
34 & 35, First link street, Nehru Nagar, off Rajiv Gandhi Salai,
Kottivakkam,
Chennai - 600 041,
India.