This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Me: Michael Randall 16Prescott@earthlink.net (USA)617-407-4244
Product: TI ADC THS1007
Connections:
01 D0 32 A1 (2.5 -> 2.9v)
02 D1 31 A2 (2.5 -> 2.9v)
03 D2 30 A3 (2.5 -> 2.9v)
04 D3 29 A4=2.5v
05 D4 28 REFIN \ 10uF -> G
06 D5 27 REFOUT /
07 Vdd 10uF -> G 26 REFP=NC
08 G 25 REFM=NC
09 D6 24 G
10 D7 23 Vdd 10uF -> G
11 D8 22 /CS0=G
12 D9 21 CS1=Vdd
13 RA0 20 R/W
14 RA1=G 19 /RD=Vdd
15 CLK 18 Vdd 10uF -> G
16 SYNC 17 G
Control Register Settings:
9 8 7 6 5 4 3 2 1 0
CR0: 0 0 1 0 0 1 0 0 0 0
CR1: 0 0 1 1 0 0 0 0 1 0
Expected Behaviour of SYNC:
H H H H H H
L L L
Observed Behaviour of SYNC:
H H H H H H H HHHHHHHHHHHHHHHHH H H H H H H H HHHHHHHHHHHHHHHHH
L L L L L L L L L L L L L L L L
=============================================
Sorry that the act of posting this yesterday
destroyed the main part of what I am having trouble with.
Here is an attempt to repair the damage . . .
==============================================
Michael Randall said:
Me: Michael Randall 16Prescott@earthlink.net (USA)617-407-4244
Product: TI ADC THS1007Connections:
01 D0 .....................32 A1 (2.5 -> 2.9v)
02 D1 .....................31 A2 (2.5 -> 2.9v)
03 D2 .....................30 A3 (2.5 -> 2.9v)
04 D3 .....................29 A4=2.5v
05 D4 .....................28 REFIN \ 10uF -> G
06 D5 .....................27 REFOUT /
07 Vdd 10uF -> G 26 REFP=NC
08 G .......................25 REFM=NC
09 D6 .....................24 G
10 D7 .....................23 Vdd 10uF -> G
11 D8 .....................22 /CS0=G
12 D9 .....................21 CS1=Vdd
13 RA0 ...................20 R/W
14 RA1=G ..............19 /RD=Vdd
15 CLK ...................18 Vdd 10uF -> G
16 SYNC ................17 G
Control Register Settings:--------9 8 7 6 5 4 3 2 1 0
CR0: 0 0 1 0 0 1 0 0 0 0
CR1: 0 0 1 1 0 0 0 0 1 0
Expected Behaviour of SYNC:=======================
L-H-H
L-H-H . . .
Observed Behaviour of SYNC:
========================
L-H-L-H-L-H-L-H-L-H-L-H-L-H-L-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H
L-H-L-H-L-H-L-H-L-H-L-H-L-H-L-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H-H . . .