Hi,
I'm very interested to use the DAC714 for 0 to +10V operation in my application. The µC there is a Micrichip PIC24FJ64GA004.
I have there one special question with the /A1, update signal. In the application bulletin "
INTERFACING THE DAC714 TO
MICRO-CONTROLLERS VIA SPI"
It is mentioned to tie the CLK to GND potential for continuous data shift and connecting the Chip-Select or Slave-Select Signal to A1 to start the updating.
When I follow this recomondations, does it work with a /SS or /CS signal when it is during data shifting low and after it, changes to high? I cannot produce a short cycle low ss or CS signal after data shifting.
Thanks for answers!
Christian