Hello.
I want to ask about real time streaming and saving data system.
The product which i saw is like this :
ADC12J4000 Evaluation Module : http://www.ti.com/tool/adc12j4000evm
ADC16DX370 Evaluation Module : http://www.ti.com/tool/adc16dx370evm
LM15851 Evaluation Module : http://www.ti.com/tool/lm15851evm
As you can see in the 'user guide', these three product have evaluation system and that system use the HSDC Pro software.
I want to know how to do the real time signal acquisitions.
In the User Guide chapter 4 (low level control), I think that 'the function which can save the binary data which show in the screen' is exist.
But I want to do this more than computer memorys.
for example,
- signal carrier is 400MHz with BW 20MHz,
- sampling rate is 4G sample / sec with 12 bit ADC
- Real time acquision with 60S
in this case the total data for saving this is : 4G * 12 bit * 60s = 2880 G bit / min = 360 G byte / min
and i want to save this binary data in my computer.
is it possible to do this by using this ADC evaluation module and HSDC Pro?
or it just save the data which showed in memory size
(I think that in this case, the real time streaming is not possible. than what is the maximum size of this possible data size? it is dependant on my computers memory size?)
Thank you for reading this questions.