This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ads1672 datasheet is missing min and max values for tCLKDR

Other Parts Discussed in Thread: ADS1672, ADS1675

Hi

Can anyone tell me the min and max values of tCLKDR (i.e. the CLK to DRDY delay)? The datasheet only list the typical value.

I will synchronize ten ADS1672. To reduce the number of interface lines I want to use SCLK and DRDY only from one of the ADCs. However, this is only possible if the DRDY (and SCLK) variations between the ADCs are not to large.

To make sure this will work I need the min and max values of tCLKDR.

BR

Vidar