Hi ,
I'm using the ADS1217 in one of our designs, we have it working well, however the initial design called for the ADS1218 and they are pin for pin compatible except for the ADS1218 having internal flash(which we are not using)
when we try to use the ADS1218, the device is not giving us correct readings, completely wrong? when we look at the two chips we see that they are identical , at least from the point of reading the internal registers, and the conversion is pretty the same? is there any difference at all between the two chips that cause wrong reading on the ADS1218?