Where can I find the setup and hold relation between WRTIQ and CLKIQ on the DAC5652A used in interleaved mode?
I cannot find any timing info in the datasheet.
Best regards
Hugo
Sr. FAE EBV
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Where can I find the setup and hold relation between WRTIQ and CLKIQ on the DAC5652A used in interleaved mode?
I cannot find any timing info in the datasheet.
Best regards
Hugo
Sr. FAE EBV
Hi Hugo,
No setup/hold times are defined for WRTIQ or CLKIQ because WRTIQ is not latched by CLKIQ or vice versa. Both these inputs are clocks and the correct timing relation to ensure reliable data transfer between these two clock domains is handled inside the DAC. The only constraint on these clocks is that their rising edge must occur at the same time or the rising edge of CLKIQ must occur before rising edge of WRTIQ. This timing relationship is described on pg 12 of datasheet under the dual bus interface mode but it should also apply for the single bus mode.
Thanks,
Eben.