Anyone know the difference between these two DACs other than price (8551 is cheaper)? We use the DAC8501 to generate audio with the ref fixed at 1.1 V and do not use the multiplying capability. Low power operation is not a requirement. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bob,
On first-order inspection the devices are remarkably similar since they are both straight forward single-channel string DACs that use external references. There are, however, several noteworthy differences between the two devices. I'll offer a comparison for you here, but fur future reference you can click here to visit a parametric table (that has several additional parameters that you may show/hide) that has a comparison feature. If you show all of the specifications and run the comparison you can get a good idea of the differences between any two products.
The short story is that in just about each DC performance parameter the DAC8551 has an edge, inclusive of drift parameters.
| Parameter | DAC8551 | DAC8501 |
| Resolution | 16-bits | 16-bits |
| Channels | 1 | 1 |
| INL (Max) | 8 LSBs | 64 LSBs |
| Zero-Code Error | Not Specified | 20mV |
| Offset Error | 12mV (Specified as "Zero-Code Error") | Not Specified |
| Gain Error | 0.2% FSR | 1.25% FSR |
| Architecture | String DAC | String DAC |
| Package | VSSOP 8 | VSSOP 8 |
| Price | $2.35/1ku | $3.12/1ku |
| Operating Temperature Range (C) | -40 to 105 | -40 to 105 |
The DAC8551 also wins in some other areas that may be of interest for your audio applications - the major carry glitch energy is lower at 0.1nV-s (compared to 20nV-s), slew rate is higher at 1.8V/us (compared to 1V/us), and digital feedthrough is lower at 0.1nV-s (compared to 0.5nV-s).
It is an oddity that the DAC8501 has specified multiplying bandwidth since this is a specification typically associated with multiplying DACs (MDACs) pretty exclusively and may be a contributor to the price difference. I cannot say for certain as I'm not involved in any pricing discussion.
In your case the DAC8551 would look to be an upgrade at lower cost. Sometimes you get to have your cake and eat it too :)