Other Parts Discussed in Thread: ADS1118
I setup a case with TI on 12/18 and have not had a response on this question. The ADS1118RUGR application report SBAA189 - September 2011 states on page4 in the last paragraph: "For extremely long thermocouples, these 1M ohm resistors may impact measurment accuracy. Increasing the resistance can alleviate these effects. Alternatively, two 1M ohm resistors connected connected as a resistor divider to one of the inputs can maitain the midpoint bias without affecting measurement results."
Using the reference diagram Figure 3 on the same page, with AIN2 and AIN3 as the inputs, is there a procedure or formula to detemine the resistor values for a particular length of thermocouple? If an off the shelf handheld thermocouple with appropriate connector with a 2 foot coiled cord were attached to this circuit how is it determined to pick the resistor values?