hi,
I am using lmp90080 to measure temperature using 3 wire RTD configuration.I Connected RTD1 to VIN0-VIN1,third line to the VREFP2 and RTD2 to the VIN2-VIN3, third line to the VREFP2. IB1 to RTD1 and IB2 to RTD2.
When I try to read both channels continuously, ADC reads incorrect values.But when I connect one RTD at a time I get the reading from the ADC perfectly.
The register settings is as follows
register value
RESETCN 0xC3
BGCALCN 0x00
CHX_CONFIG(0x21) 0x76 for CH0
CHX_CONFIG(0x25) 0x76 for CH2
RESTART 0x01
ADC_AUXCN 0x0A
CH_SCAN 0x82
CHX_INPUTCN (0x20) 0x41 for CH0
CHX_INPUTCN(ox24) 0x65 for CH2
Help me out with this..
Thanks and Regards
Anbu