Hi there,
I'm designing a circuit which uses an ADS1222 to perform 16-bit ADC conversions out of an inclinometer (SCA103T for what matters).
The circuitry includes two reference voltage IC's: REF5025 as the analog reference for the ADS, and REF5050 as the voltage input for the sensor.
I've seen a lot of examples using OpAmps in two different stages of such circuits:
- Between the sensor output and the ADC input;
- Between the voltage references output and the inputs of those two components.
As per the datasheets, the REF50xx is able of supplying 10amp. The sensor requirement is 4amp. Would I really need a buffer before it on that situation?
The power requirement for the ADS1222 is much lower than that, and again is seems that the REF should be easily able to supply the required juice.
Do we gain something by using the buffers? Or are we rather adding complexity, errors, offsets, etc? If the OpAmps are a benefical addition, is my initial choice OPA2335 a good option?
Thanks!