Hi,
I have an ADS1293EVM board and have successfully used it with gel-type electrodes to get 3-lead ECG readings. I am experimenting with the use of dry-contact sensors to develop a wearable ECG sensor. Specifically, I am attaching PS25251 EPIC Ultra High Impedance ECG Sensor and connecting them via two 3.7V batteries to get the dual polarity ( +- 3.7V). Here is the datasheet of the sensor:
Connections from the EPIC sensors via shielded cable are as follows:
VDD to +3.7V battery
VSS to -3.7V battery
GND to Board GND
Signal to IN1A
I am getting a lot of noisy spikes on the ADS1293 signal trace and cannot seem to tune the ADS1293 to accept the new sensors. When I go back to the gel-electrodes, the ADS1293 works fine.
Can you recommend what parameters (registers) need to be changed to make these electrodes work with the ADS1293?