Hi,
I would like to ask you some questions about OVR_SDOUT of ADS4146 as below.
Q1) The timing
I suppose there is not a detailed timing of this signal on the datasheet when this pin is used as "status signal".
Could you tell me the timing? For example, ON/OFF timing, minimum pulse width(clock, Hz), etc
And this signal is outputted by up-edge of CLK/M signal (=synchronized with input clock), right?
The max signal frequency of this signal is 20MHz which is SCLK frequency, right? (in case of used as status, not interface.)
I am planning to use ADS4146 as 130MHz DDR mode.
Q2) SIgnal level sift
I am considering to use SN74LVC1T45 to change the signal level (1.8V to 2.5V or 3.3V).
Is this possible to use?
Thank you for your support in advance.
Best Regards,