This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7678EVM I2C Interface with Raspberry Pi



I have this code for I2C Interface.Is this correct for DAC 7678EVm,but I am not getting Output on the DAC Channels. The code takes the data,but how to see any waveform in the Oscilloscope , Please Help.

Please Help me.

#include <wiringPiI2C.h>
#include<wiringPi.h>
#include <stdio.h>

//unsigned char test[2] ={0};
int fd;
int i=4095;
int dID = 0x48;

int main(void){
        printf("check1");
int j;
        if((fd=wiringPiI2CSetup(dID))<0){
                printf("error opening i2c channel\n\r");
                return 0;
        }
        wiringPiI2CWrite(fd,0x80);
        wiringPiI2CWrite(fd,0x00);
        wiringPiI2CWrite(fd,0x00);
        //void digitalWriteByte(0x88);
        //void digitalWriteByte(0x40);
        sleep(1);
        if((fd=wiringPiI2CSetup(dID))<0){
                printf("error opening i2c channel\n\r");
                return 0;
        }
        if(wiringPiI2CWrite(fd,(0b00001111))<0){
                printf("ERROR 1");
                return 0;
        }
//      for(i=0; i<1000; i++){
while(i--){
                if(wiringPiI2CWrite(fd, 0b11110000)<0){
                        printf("ERROR 2");
                }
                if(wiringPiI2CWrite(fd, 0b11111111)<0){
                        printf("ERROR 3");
                }
                printf("Success: %d \n",i);
                for(j=0 ; j<100000; j++);
                wiringPiI2CReadReg8(fd,0b00001111);
                wiringPiI2CReadReg8(fd,0b11110000);
                //sleep(1);
//      }
//if((e= wiringPiI2CWrite(fd,23))<0){
//printf("error writing to slave\n\r");
//}else{
//printf("writing hex:0x%i size:%i\n\r",test,sizeof(test));
}

sleep(1);
return 0;

}