Other Parts Discussed in Thread: DAC7563, DAC8563, OPA140, TPS7A30, DAC8165
Hi,
I am trying to configure the DAC7563. I can write correctly to the DAC-A and the DAC-B. But in the init the DAC7563 has the default values of 0V on the DAC-A and DAC-B.
According to the datasheet the code DAC7563 is the mid-scale, so in the initial state the DACs will have to supply 2.5Volts, won't they?
Connections:
1- VoutA -> oscilloscope
2- VoutB -> oscilloscope
3- GND -> GND
4- LDAC -> GND
5- CLR -> 3.3V
6- SYNC -> CS (uController)
7- SCLK -> SCLK (uController)
8- DIN -> MOSI (uController)
9- Avdd - > 3.3V (with capactior 1uF)
10- Vrefin/Vrefout -> capacitor 470nF
Thank you so much. Best regards.
1º- VoutA -> oscilloscope