This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5681 gain drift

Other Parts Discussed in Thread: DAC5681

I'm looking into a high speed DAC for an Infrared projector. I need 14-16 bits of DC accuracy and a full scale settling time of around 100ns down to 1LSB. The DAC5681 looks promising but I have a question about the gain and offset temperature drift. I'm comparing this part to the Linear Technology LTC2000 which has a typical gain drift specification of 5ppm/degree C listed on page 5 of the data sheet, however, a chart on page 9 of the data sheet shows gain error vs temperature and indicates this error is more like 100ppm/degree C between 25 and 50 degrees C where the device will likely operate in an ambient environment. At lower temperatures the gain drift matches the typical specification.

The DAC5681 list typical gain drift errors of 15ppm/degree C without internal reference and 30ppm/degree C with internal reference. Is there a curve or data available showing gain drift with temperature so I can see that the relationship is fairly linear over the temperature range for the DAC5681 or if there are areas where the gain drift is worse? Thanks.

  • Hi Larry,

    The gain drift spec mentioned in the datasheet is not correct.

    Here is gain drift spec over temperature.

     

    Internal Ref

    External Ref

    Temperature

    Drift (ppm/c)

    Drift (ppm/c)

    -40

    0

    0

    -20

    197

    103

    0

    181

    100

    15

    167

    97

    25

    163

    98

    45

    144

    92

    65

    125

    85

    85

    112

    79

    Regards,

    Neeraj Gill