I am not sure if this is the right forum for this question but I figured i would put it out there just in case. I am working with a DAC084S085 digital to analog converter. It is a 4 channel DAC, but I am using only 3 channels, (A, B, and C). I am interfacing with the IC using SPI. I have successful comms because I can change the output of channels A and C successfully. But for some reason if I set channel B to anything other than zero it affects the outputs of channels A and C attenuating them significantly. Is this normal operation? What is causing channels A and C to be affected when i try to set them to anything other than 0? Can the DAC be configured to use 3 of the 4 channels or if a channel is not used does it need to be physically tied to a load and driven so the op amp functions normally?