I am using the space qualified part. I have two layout questions.
The datasheet says "the center die attach pad of the device should be connected to ground with low inductive path." Does this pad need to be soldered for best performance?
Also I am using a single ground plane. The datasheet says
"the key is to make sure that the supply current in the ground plane doe not return under a sensitive node. This is done by routing a trace from the ADC to the regulator so it does not run under a critical node." Isn't this the same of splitting the ground plane? Should it be a separate wide trace to the regulator bulk capacitor and connecting to ground there? This is my first ADC circuit.