Other Parts Discussed in Thread: ADS8344
Hello everyone,
I have one problem which is inconceivable to me. I have read very much documents about ADC's before i make a final design for my board. There wasn't any description about that one problem. So here are the questions:
1. How can i divide an input voltage (e.g. with reference 2.5V on ADS8344) to reach exactly the rails of the reference voltage? I mean i will loosing some read-bits because it is not possible to reach the reference input exactly (e.g. i will reach only 2.48V). So there aren't really =16bits available.
2. Is a simple voltage divider at the input conceivable (with ADS8344)?
Best Regards,
Sebastian