The AMC7891 MAC device contains an ADC which has an automatic 500 kHz clock mode. The device has a signal to noise ratio of about 61 dBc at Fin = 1 kHz (I assume that is at 500 ksps), so the clock fidelity should be fairly good. How is this clock derived and what is the tolerance on the sample clock?
I would like to try and sample an audio waveform with this clock; would the sampled fidelity be better using this internal clock or should I sample using the manual trigger and external (clean, high stability) clock on the SPI bus? I would prefer the latter because it is synchronous.