Hi,
I have some problems for using ADS8332.
I want to use manual channel select and Auto trigger mode. How can I select channel 2?
I code somethings, but it is error.
First, I give the convst pin high.
Second, I send the 'write CFR' code: 0xE000.
Delay 16-clock(70ns).
Third, I send 0x2000 to select channel 2
Delay 16-clock(70ns).
Fourth, I send 0xD000 to read CFR.
Delay 16-clock(70ns).
Then, I give the convst pin low.
and write a while loop to determine the EOC pin, if EOC is LOW, start to get data.
and, give the convst pin high.
that's all,
The result I only get data from channel 0 (first channel).
I don't know that why is not from channel 2.
And the conv pin do I need to configure it?
Can you help me?