I'm designing this schematic about TLC7524, Unipolar Operation
Could you clarify this information about GAIN adjustment: datasheet pg7 "RA and RB used only if gain adjustment is required" but not specify anything
- Input 250=> D7...D0 [1111 1010]
- Vout 10V
- Vref= -1.5V
- R19= 732Ohm??
- R21 = 5K Ohm
Is Correct this assumption?
Vout= -Vref * R21/R19 * (D7/2+...+ D0/256) = 1.5 * 5000/732 * 250/256 = 10V
Thanks a million