hi all
I need measure dc voltage from array of solar panels. this voltage is Vmin= 75V and Vmax=125V. I will use the amc1304M25 for this work.
I have read the application note SBAA215, saying that lower shunt resistor, lower offset and gain error. why in the reference design place a big resistor increasing gain error above of 10% ?. is for currents issues?, or why issue?
I plan to use a shunt resistor of 100 ohms and series resistor of 50K. this values are ok?