Other Parts Discussed in Thread: DAC8560, LM358
Hi,
We are following the reference design "Bipolar +/-10V Analog Output from a Unipolar Voltage
Output DAC" from TI for using DAC8560 with OPAMP. In our circuit the following changes we have done
1. We have used LM358 OPAMP
2. We are using OPAMP in Non-inverting amplifier mode since we need unipolar output in the range of 0 - 8 V , DC.
3.In the schematic OPAMP circuit is shown in summing amplifier mode but in the board resistor R14 is not populated.
During the testing we observed that when we connect this circuit to DC drive (input : 0 - 8 V DC, Output : 0-180 V DC) the 5 amps fuse in the DC drive gets burned. I herewith attached our schematic diagram for your reference.
Please provide a suitable solution.