This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4245 VCM output

I am using ADS4245EP Analog to Digital converter in my design with differential input signal and single ended clock. I am operating only one channel(channel B) in 2's complement parallel CMOS mode.At the initial power up of the ADC ,Clkout signal from ADC remains high and VCM shows 200mV instead of 0.95V.I have followed design from the datasheet for my schematic. Please suggest a suitable solution to my problem.Pins sel include(SDATA,SEN,SDOUT:ground and RESET,SCLK:high and cntrl1,cntrl2,cntrl3:101 respectively).