This has been an ongoing issue. Replacing the chip fixes the problem.
Here is a scope trace of the register write measured at the ADS1212 pins...
When I read it back, the bit is zero....
(I have a long ground lead on my scope probe. It's not as noisy as these traces would suggest.)
This is not intermittent. This part does it every time. I checked the DRDY line and the A/D data rate matches the register settings I read back. Unfortunately, it's the wrong rate. It appears that on some chips, bit zero of byte one (DR8) cannot be changed from it's default value of zero.
I have a 2MHz clock rate.
I can hang onto this board for a couple of weeks if there is something you would like me to try.
Thanks,
Chris