Other Parts Discussed in Thread: LMP90100
Hi
I am using LMP90100 and able to configure and read output from the ADC. I'm using 5V for VREF and also for adc supply.When i give 1V between VINP-VINN i was able to read 0.99-0.98 but sometime it reading voltage as 1.65(at least twice in every 10 times).
I also configured the adc as 214SPS and gave square wave of period 2s from FG. When i read the output data i only got approximately 160 highs and lows instead of 214 highs and lows.
I have attached the output log file where you can see the result I got.you can also see the variation in the output log which is highlighted.
ThanksLMP901001Channel214SPS.xlsx
Prakash Ramamoorthy