Hi all,
Would you mind if we ask ADC08131BIN?
Of course, we know that ADC08131BIN is EOL, so this question is relation to only existing system.
<Question1>
Does VrefC of ADC08131BIN receive 5.0V?
Or, the datasheet shows "For the ADC08131, the output of the on-board reference is internally tied to the reference input."
So,Vref is 2.5V, isn't it?
<Question2>
It is relation <Question1>, if VREFC can accept 5.0V, can SDO output 5V(in case of Vin+=5V)?
Kind regards,
Hirotaka Matsumoto