Hello Everybody,
We want to evaluate the performance of the ADC08D1000 but we have some troubles to reach the performance of the device. The component is soldered on ROGER R007 PCB board.
The PCB Board is realized in four layers ( include two ground planes), all the decoupling capacitors are closed to the device. three balun ADT2-18 are used for the clock, channel I and channelQ.
All the LVDS output line are matched in lenght and line impedance (50ohms) terminaison (100 Ohms).
All the input Line are matched in lenght and line impedance (50Ohms).
We used LPF 1GHz for the clock and LPF 250MHz for the channels.
Setup of the device
Input: AC Coupled
VCMO=Low
PD=PDQ=Low
Output: DDR
VBG=Floating
Rext=3.3K-0.1%
FSR=High
CalDlyDESSCS_=Floating
OUTV=High
DCLK_RESET=Floating
QUESTION:
When we setup the level for the clock to 600mVpp / 1GHz differential, with no signal in channel Q and Channel I, we have an offset at the LVDS outputs. Instead having code 127 or 128, we have code 132 or 119. Can you give us some suggestion to fix the problem?
Thanks for your help.