Other Parts Discussed in Thread: ADC07D1520
Hello,
I'm designing a new module with 4 chips ADC07D1520, and one FPGA, and I'm using the ADC0xD1520RB as reference.
Looking at the ADC0xD1520RB schematic page 11, it seems to me that the ADC power 1V9A comes up some 55ms after 1V8IO power, which supplies the FPGA ADC IOs.
Is that correct?
If that is correct, the ADCs connect to the FPGA, and the FPGA IOs come to life sooner than the ADC is powered, right?
This appears to be in contradiction to the ADC07D1520 data sheet, which states at page 44:
"Be sure that the supplies to circuits driving any of the input pins, analog or digital, do not come up any faster than does the voltage at the ADC07D1520 power pins."
Is that a mistake in the DB schematic, or what am I missing here?
Anyway, I'm thinking to power the Vdr of the ADC07D1520 at the same 1.8V power rail as powers the corresponding FPGA IO bank, and to start this 1.8V power only after the FPGA core power comes up. So, the Vdr will come up later than Va for the ADC chip.
On the other hand, Va will start without delay, and after Va is up, the Front End power gets enabled.
Please, give me your opinion about this option.
Thanks,
MIrcea