Hi,
I am working on ADS1296R with MSP430 to get ECG data.
I have followed PACE detection circuit from TI reference (by Tony Calabria).
After few trial and error with the resistor and capacitor values, I am able to detect a pulse of duration 0.1ms and above & 4mV and above.
1. Problem - When i see the GPIO pin on the CRO, i see a spurious pulse along with the PACE pulse from the simulator.
This pulse occurs even when the simulator is OFF. It occurs every 1.3 second.
2. Also, i would like to bring down the detection threshold voltage to 2mV (currently circuit can detect 4mV and above) as suggested in the document
Thanks
Arun