Other Parts Discussed in Thread: ADS4245-EP, ADS4245
Hi sir,
I am using a ADS4245-EP and i have problems... With my 6 first prototypes, 3 are working well and 3 other doesn't work...
First 6 prototypes have AD4245-EP from same batch.
The problem seem to be VCM load at power up.
Remember, in data sheet, it is written VCM output current capability typ. 4mA.
In my schematics, VCM is loaded with arround 1K (0.95mA).
What i have seen;
- If VCM is loaded with 1K at power up, VCM fall and ADC never start.
- If VCM is not loaded at power up and after 1K is load, ADC work.
Can i have a detailed synoptic of VCM circuitry to understand?
Does VCM pin scan something at power up or is there some protections?
Best Regards.