Other Parts Discussed in Thread: TRF3765, ADC12J4000EVM
Hi my csuotmer asked:I would like to find out from TI what they believe to be the main difference between the ADC12J4000EVM and the TSW12J54EVM? And why thy would suggest one above the other? My main aim is to drive the ADC using a differential input, bypassing most of the analog input circuitry. I also have to supply the actual ADC clock externally. I’ve seen in the documentation that this can be done, but then you need to supply both Fs as well as Fs/2? That is not great, because then I would need to derive the one from the other? Won’t it be possible to just the EXT_VCO and drive it with 4 GHz with the correct settings of the TRF3765 on the evaluation module?