This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Input impedance matching ADS131 (or other if better) with TIPD118

Other Parts Discussed in Thread: ADS131E04, OPA376, TIPD118, ADS130E08, OPA735, OPA335

Hello,

I've found very useful circuit design in your resources: http://www.ti.com/tool/TIPD118#1

I have a prototype with ADS131E04, single supply AVDD=5V, internal Vref=4V also taken out from Vref+ and divided by 2 and buffered to provide CM of single ended input.

U1=OPA376, R1=36k, R2=14,3k, C2=1200p, R4=62, C9=100n 

I usually notice about -7 value when nothing is connected to input circuit. I assume it is caused by not matched input impedances, am I right? How should I calculate IN- branch? I have used same 62R + 100n as low pass filter but it's sourced from "+" terminal of U1, which is sourced from buffered Vref/2 via 1k + 1uF.

This effect can be seen regardless of OFFSETCAL opcode using so I assume this command is executed with disconnected IN+/IN- inputs and can't compensate that.

I'm mostly interested in signals from range 10..2000Hz but I usually use 8ksps, 16bit is enough.

Or maybe there is another ADS better suited for 4 single ended signals?